I want to use the example of the RS485 in
C:\Freescale\Freescale_MQX_4_1_TWRK64F120M\mqx\examples\rs485\build\iar\rs485_twrk64f120m.
But The data type is string char data_buffer[] = "RS485 send example";
If I want to send and receive a number data with BYTE type.
For example. 0x01 0x02 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x10.
BYTE data_buffer[10];
data_buffer[0]=0x01;
data_buffer[1]=0x02;
data_buffer[2]=0x01;
data_buffer[3]=0x01;
data_buffer[4]=0x01;
data_buffer[5]=0x01;
data_buffer[6]=0x01;
data_buffer[7]=0x01;
data_buffer[8]=0x01;
data_buffer[9]=0x10;
The master sends the data in the data_buffer[10] and the slaver receives the data data_buffer[10].
It is very easy to write the source code without OS. But I do not know how to do in the MQX.
How to realize it in the MQX ?
Solved! Go to Solution.
Hi Robin:
I think you can transform the string into byte. you can do it in rx or tx side.
Have a great day,
Daniel
Hi Robin:
I think you can transform the string into byte. you can do it in rx or tx side.
Have a great day,
Daniel