Is KDS compatible with Eclipse Luna?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is KDS compatible with Eclipse Luna?

Jump to solution
560 Views
davepfaltzgraff
Senior Contributor I

For an unrelated project, I've installed the Luna release of Eclipse. This leads to several questions:

 

1. Can I run the KDS in Luna?

 

2. If so is the installation of KDS any different?

 

3. If not, can the Luna and Eclipse releases coexist?

 

Thanks

Labels (1)
Tags (3)
0 Kudos
1 Solution
374 Views
BlackNight
NXP Employee
NXP Employee

1. No. KDS comes with its own Eclipse (Kepler) and is tested with it.

2. See 1. Because the Processor Expert plugin and components do not run in Luna (yet).

3. Yes.

Erich

View solution in original post

0 Kudos
1 Reply
375 Views
BlackNight
NXP Employee
NXP Employee

1. No. KDS comes with its own Eclipse (Kepler) and is tested with it.

2. See 1. Because the Processor Expert plugin and components do not run in Luna (yet).

3. Yes.

Erich

0 Kudos