AnsweredAssumed Answered

Unable to use penmount touch serial driver in LTIB

Question asked by nishad kamdar on Sep 20, 2014
Latest reply on Sep 21, 2014 by igorpadykov

Hello all,

 

I have a penmount serial touchscreen which I wish to connect to my iMX6Q custom board using the serial port at ttymxc0.

 

My ttymxc0 is working correctly.

 

I enabled the penmount serial driver in the kernel configuration to be built in module.

 

I can see the penmount.ko module built.

 

However, when I connect the Touchscreen using the serial port to my board, the touch doesn't work.

 

The screen works with a Ubuntu PC using Serial port, one I install the drivers and calibrate it.

 

What should i do to get it working with my board.

 

Thank you for your time,

 

Nishad

Outcomes