In MQX4.1 mfs\source\generic\part_mgr.c, function below calls _nio_dev_uninstall() but IAR Linker complaints about "no definition for "_io_part_mgr_uninstall".
int32_t _io_part_mgr_uninstall
(
char *identifier /*[IN] The identifier string of the device */
)
{
return _nio_dev_uninstall(identifier);
}
I can't find the definition for _nio_dev_uninstall() from MQX4.1. In MQX3.8, it was _io_dev_uninstall(). Can anyone help on the definition of this function?
thanks!
Hui
Solved! Go to Solution.
Thank you for your bug report.
Yes, it is known bug and it was already fixed at development branch.
Correct line is:
return _io_dev_uninstall(identifier);
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your bug report.
Yes, it is known bug and it was already fixed at development branch.
Correct line is:
return _io_dev_uninstall(identifier);
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------