Hi, I am working with TWR-K60D100M board. I want to run FNET bootloader on the specified board. But I can't find any FNET demo for TWR-K60D100M. Is there any FNET demo available for TWR-K60D100M. I am using CW 10.5 and MQX 4.1.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, I am working with TWR-K60D100M board. I want to run FNET bootloader on the specified board. But I can't find any FNET demo for TWR-K60D100M. Is there any FNET demo available for TWR-K60D100M. I am using CW 10.5 and MQX 4.1.

413 Views
saranyaraveendr
Contributor I

Hi,

I am working with TWR-K60D100M board. I want to run FNET bootloader on the specified board. But I can't find any FNET demo for TWR-K60D100M. Is there any FNET demo available for TWR-K60D100M. I am using CW 10.5 and MQX 4.1.

0 Kudos
1 Reply

238 Views
RadekS
NXP Employee
NXP Employee

TWR-K60D100M isn’t directly supported by FNET.

However there should not be big differences in compare with TWR-K60N512. Most important changes will be probably in:

  1. Clock setup – PLL settings
  2. UART pins configuration.

Detail information about differences between Kinetis K60 Rev1.x (TWR-K60N512) and Rev2.x (TWR-K60D100M) could be found in our application note AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide:

http://www.freescale.com/files/32bit/doc/app_note/AN4445.pdf


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos