i.MX6Dual's system with battery.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Dual's system with battery.

Jump to solution
576 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I'm considering i.MX6Dual's system with Li-ion battery.

Could you tell me how to detect the remaining battery level by i.MX6?

Best Regards,

Keita

Labels (4)
0 Kudos
1 Solution
496 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

one can add to design small adc with control over i2c/spi/uart or

use special devices lke below

Analog Devices Introduces Lithium-Ion Battery Monitoring and Protection System for Energy, Industria...

Best regards

igor
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
497 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

one can add to design small adc with control over i2c/spi/uart or

use special devices lke below

Analog Devices Introduces Lithium-Ion Battery Monitoring and Protection System for Energy, Industria...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos