AnsweredAssumed Answered

802.11 Wireless Recommendations

Question asked by Kenny Koller on Sep 14, 2014
Latest reply on Sep 17, 2014 by Radek Sestak

Hi,

 

I've been using the Freedom K64 to bring up firmware for a start-up and it has been going well with MQX, TAD, and the support I have received here.

 

This week I was asked to help build a prototype for a very large company that it is interested in testing the market for Internet of Things. The other project requires most of my bandwidth but if I can leverage what I have built on top of MQX on Kinetis I can imagine pulling it off. I'm assuming that if the wireless driver has been properly integrated that my socket code will be the same.

 

I'd like to use an existing demo platform as a reference for a custom for custom PCB. I've looked at the TWR Atheros 4100 and it looks to mate with a K60 board of some kind. Anyone have experience with this?  Is this platform stable and reliable?

 

Prefer to use IAR and hoping that a BSP is ready to go. Given that is TWR I'm thinking this is all very doable.

 

Thanks,

 

Kenny

Outcomes