AnsweredAssumed Answered

Basic Text Overlay

Question asked by alex martins on Sep 11, 2014
Latest reply on Sep 17, 2014 by jamesbone

Hello everyone,

 

Brand new to this board, and engineering in general, so please bear with me

 

Basically I would like to know where I need to look in order to add text overlay to a video - I've looked at the Image Processing Unit (IPU), Gstreamer, and the PiXel Pipeline (PXP) and have seen some things in there that may help but I'm getting bogged down and confused with all the information that is there. If somebody could narrow down where I need to look in order to do this that would be great.

 

Here is a description of the application that I am using this for. Basically we got this DVR that is using the iMx6 Solo processor. I am designing a board that interfaces with this processor using UART communications. The board I'm designing will receive command either from a keyboard or membrane switch and based off this change some settings. An example would be a button on the membrane switch which will cause a menu to be displayed on the screen. Not looking to do anything fancy with it right now, just want the UART command that is sent to the IMx6 to turn the menu on/off and to navigate through it.

 

If you need more information please don't hesitate to ask.

 

Thank-you and I look forward to your replies.

Outcomes