AnsweredAssumed Answered

Problem with multiple targets in CW 6.0

Question asked by tombednarchuk tombednarchuk on Sep 12, 2007
Latest reply on Feb 29, 2008 by Alex O'Donnell
Hi! I'm trying to set up my CW project to have 2 targets for the EL32 processor.

1 target will be for the initila development hardware (EL32 demo board and off board hardware) and the other target will be for the production hardware. The main differences are the ports used to drive the external hardware.

If I try and create a new target with CW 6.0, the selection is greyed out but it can be selected in the previous version (4.6 ??). Is this a bug or is something else interfering?

Is the workaround to develop in the previous version??

Thanks,

Tom

Outcomes