Mohamed Othman

HCS12 MSCAN identifier question

Discussion created by Mohamed Othman on Sep 12, 2007
Latest reply on Jul 21, 2009 by yadunandankasu yadunandankasu
Hello,
I have a quick question about CAN identifier in HCS12 MCU.
When it says in some documents that the ID of the message is "23f" (I assume this is a hex), then:
1. is this means 0x023f or 0x23f0 ?
2. where is the first bit? is it left justified or right justified?
3. As the bits in the acceptance ID registers will be sorted from IDs0 to ID 28, Can anybody please
,as an example, tell me how would the four Acceptance registers look like when filled with the stated acceptance ID (23f)?
 
thank you,
 
 

Outcomes