Good morning,
I use K60 with MQX4.0.2 and CW14. I compiled my software in debug mode and try to debug it.
I implemented a webserver. My debugger is the PE Multilink Universal.
If I run the software without debugger, the webserver will work normally.
If I run the software using the debugger, the webserver and also the ping command will not working.
By Task summery window I see on TCP/IP task, the message: Rx Msg Blocked, Timeouted!
Why?
Does the debugger work with TCP/IP connection?
I use the initialization of the webserver example.
Best Regards
Mirko
Solved! Go to Solution.
The debugger can work with TCPIP connection.
The web server demo can work well with debugger in TWR-K60 board.
Maybe you need to check whether it is a hardware issue or not.
Have a great day,
Daniel
The debugger can work with TCPIP connection.
The web server demo can work well with debugger in TWR-K60 board.
Maybe you need to check whether it is a hardware issue or not.
Have a great day,
Daniel