ruikun jiang

CW8.6 MPC8548E - I met a problem when burning Uboot to Flash from CodeWarrior.

Discussion created by ruikun jiang on Sep 12, 2007
Latest reply on Sep 13, 2007 by Thierry Giraud
I want to burn the U-boot boot loader to Flash from CodeWarrior. When I erased the sectors of Flash, the CW told me it failed. The failing infomations are as follows.
         'Flash Programmer: Can not initialize the target: "8548" Please make sure "C:\Program Files\Freescale\CodeWarrior PowerPC Comm V8.6\PowerPC_EABI_Support\Initialization_Files\PQ3\8548EP8548_init.cfg" exists and it is a valid configuration file.  Additional error information: Interface function IMWProtocol::GetPreference is unimplemented.'
         The targeting cpu is MPC8548E. The targeting board is EP8548A. The CodeWarrior is V8.6.
 
 
please help.
thanks.


--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.



Message Edited by Alban on 2007-09-12 12:06 PM

Outcomes