NMI Pin Tab missing on KDS 1.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NMI Pin Tab missing on KDS 1.1.1

Jump to solution
725 Views
normansiegel
NXP Employee
NXP Employee

I am running the latest version of KDS (1.1.1) and KSDK (1.0.0), and the NMI Pin tab is missing.

 

This first image is from an older version of KDS:

14550_14550.pngNMI tab.png

 

This second image is from KDS 1.1.1

 

14551_14551.pngNMI pin tab KDS 1.1.1.png

 

Thanks!

Norm

Labels (1)
Tags (2)
0 Kudos
1 Solution
495 Views
BlackNight
NXP Employee
NXP Employee

I see from your screenshot that you have added the Kinetis SDK to that project.

For SDK, the NMI pin is handled in the pin muxing, not in the CPU component.

Erich

View solution in original post

0 Kudos
5 Replies
495 Views
BlackNight
NXP Employee
NXP Employee

Hi Norm,

I think you are looking in the wrong place, it is here:

pastedImage_0.png

You do not have the left pane expanded.

In any case, you can search for a setting, see

http://mcuoneclipse.com/2014/06/24/finding-settings-in-processor-expert-components/

Erich

0 Kudos
495 Views
DavidS
NXP Employee
NXP Employee

Hi Erich,

I have same results as Norm.

When I open KDS1.1.1 to a File-->New-->Kinetis Design Studio Project that is PE enabled, I do not see the "Common settings" listed.  Picture below.

Could some update be missing?

Could it be issue with new projects?

ScreenHunter_70 Sep. 03 11.37.gif

The Search did not find anything related to NMI either.

Regards,

David

0 Kudos
496 Views
BlackNight
NXP Employee
NXP Employee

I see from your screenshot that you have added the Kinetis SDK to that project.

For SDK, the NMI pin is handled in the pin muxing, not in the CPU component.

Erich

0 Kudos
495 Views
normansiegel
NXP Employee
NXP Employee

Thanks Erich.

Regards,

Norm

0 Kudos
495 Views
DavidS
NXP Employee
NXP Employee

So many rules.

Thank you Erich.

Regards,

David

0 Kudos