It is true that there are some differences between the spec documentation of the board and the flash chip that is on the board but regarding the user they are compatible. Therefore I advise you to edit your 8349ITX_rev1._FLASH.xml file from CW 8.8 installation folder\bin\Plugins\Support\Flash_Programmer\EPPC\83xx directory that is specifying the algorithm too as in the attached screenshot and I hope everything will be OK (see the attached 8349ITX_rev1_FLASH_xml.JPG):
<flashconfwindow>
<membaseaddr>0xFF000000</membaseaddr>
<device>AM29LV128ML</device>
<organization>8Mx16x1</organization>
<flashstart>0xFF000000</flashstart>
<flashend>0xFFFFFFFF</flashend>
If still not working, please log a service request here. Thank you.
If you cannot find your device in the Flash Programmer list of the CodeWarrior Power Architecture 8.8 then you can choose a similar flash from the Flash configuration panel if available or you can add your flash type yourself to Flash Programmer.
There is an application note and easy to use Perl script on how to add your own flash devices to Flash Programmer. You can find them in:
http://www.freescale.com/files/soft_dev_tools/doc/white_paper/CWFLASHPROWP.pdf
CodeWarrior PA installation folder\PowerPC_EABI_Tools\FlashProgrammer\flash_entrygen.pl
I hope this helps.
This board is currently not supported in the Codewarrior Power Architecture 8.7. The support for this board will be added in the 8.8 version for which the work is in progress. Currently there is no any 8.8 beta version available for customers that contains the support for 8349E-mITXE board. Please check periodically with your Freescale provider when a CW PA 8.8 beta version with 8349E-mITXE support will be available for customers.
Thank you for your understanding.