About the HEAC function of HDMI1.4 of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the HEAC function of HDMI1.4 of i.MX6

Jump to solution
660 Views
yuuki
Senior Contributor II

Dear all,

Is HDMI1.4 of i.MX6 supporting the HEAC function?

The keyword of HEAC is indicated to the reference manual.

IMX6DQRM.pdf rev2:
- Figure 33-1. HDMI Block Diagram
- 33.5.280 Main Controller HEAC PHY Reset Register(HDMI_MC_HEACPHY_RST)

However, I think that the pin used by HEAC is not enough.

May I have advice?

Best Regards,

Yuuki

Labels (2)
Tags (3)
0 Kudos
1 Solution
530 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

HEAC is not supported.

Best regards

chip
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
531 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

HEAC is not supported.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos