AnsweredAssumed Answered

Is there a sample project for the MC56F84789 device that illustrates use of STOP instruction? (Yes, and I include this below)

Question asked by John Winters Employee on Sep 2, 2014

Yes, the halt and wait are illustrated in the attached zip file which is a zipped project for CodeWarrior 10.6.

It runs on the Tower module for the MC56F84789.

 

Note, most of the work is done with the GUI and Processor Expert.

 

Note that since I used a timer, I can make this time stop or keep running in PEx depending on how I configure the CPU component.

 

Right now, it is set for keep running.

 

Can you make it STOP during STOP mode?

Original Attachment has been moved to: Haltish.zip

Outcomes