AnsweredAssumed Answered

TWR-S12GN32 - Multilink

Question asked by Anthony Schnelle on Sep 1, 2014
Latest reply on Sep 2, 2014 by Anthony Schnelle

Hey,

 

I was wondering if anyone had successfully programmed the TWR-S12GN32 board using the 6 pin BDM port? This is my first time working with a Freescale microprocessor and ultimately need to be able to program an S12GN32 on a custom PCB design which won't have a built in programmer. I can program this board just fine using the OSBDM over USB connection but can't connect using a Multilink programmer and CodeWarrior 5.1, if anybody had some advice that would be greatly appreciated.

 

Anthony

Outcomes