AnsweredAssumed Answered

The DCD table for u-Boot of iMX28_Linux BSP

Question asked by yuuki on Aug 28, 2014
Latest reply on Aug 28, 2014 by igorpadykov

Dear all,

 

Our customer changed the following pin into the PWM output in the original board.

L7 pin => PWM1
K8 pin => PWM2

 

However, a pulse signal is outputted from these pins during the Boot.

 

On a MX28EVK of Freescale, these pins are DUART_TX and BACKLIGHT_PWM.
Their BSP is based on Linux_BSP of Freescale.

 

I think that they need to change a setup of these pins in U-Boot.

I understand that such a setup is performed by DCD table.

However, I was not able to find DCD table in Freescale Linux_BSP.

 

Would you teach the place where DCD tabel is indicated who sets up these pins?

 

Best regards,
Yuuki

Outcomes