I'm trying to install codewarrior on my win7 64 PC, I recently posted getting some help regarding installing CW on another PC and got the following replies which were very helpful.
https://community.freescale.com/thread/329298
So that got us up on running on both Windows XP and Windows 7 which we needed.
However I've now tried to reproduce this setup on my own Windows7 64 development box. However it was not a success (it connected and talked to the tap but gave some other error which I now forget) but during this process I decided to uninstall and repeat my steps to make sure I took the correct patches etc etc.
However when I now try reinstall I get the following error....
In addition the installation window has the following in it
The same steps seem to have worked elsewhere so is this a 64 bit windows problem or is it something else...
thanks in advance
regards
Craig
Solved! Go to Solution.
Tou can try to follow the steps from ccs\drivers\ccs_drivers_installation_help.txt.
Adrian
Thanks Yiping for your advice, however I definitely did not have the device plugged in during this process.
I did however have another device plugged in, I wonder if perhaps that confused the installer somehow?
I'll try with absolutely nothing plugged in.
Thanks for your reply.
Tou can try to follow the steps from ccs\drivers\ccs_drivers_installation_help.txt.
Adrian
Thanks Adrian
Followed the uninstall steps for the USB driver and all is well again, at least on the install front. Now I need to see if it'll talk to my target!! but that's another story.
Hello Craig,
Please note don't plug in USB TAP during CodeWarrior 8.8 or any patch installation.
I think probably that is the cause.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------