imx6 - Operating Ranges & Absolute Maximum Ratings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 - Operating Ranges & Absolute Maximum Ratings

908 Views
Ansari
Contributor IV

Dear sir/madam,

We are using imx6Q sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.

We have referred below document for operating ranges & absolute maximum ratings.
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf


 
We would like to know, If the chip runs at 1.2GHz then what is the operating range & absolute max. rating of below symbols.
VDD_ARM_IN

VDD_ARM23_IN

VDD_SOC_IN
VDD_ARM_CAP

VDD_ARM23_CAP

VDD_SOC_CAP

VDD_PU_CAP


Thank You,
Regards,
Ansari

0 Kudos
1 Reply

532 Views
gusarambula
NXP TechSupport
NXP TechSupport

I apologize for the omission on the datasheet. As far as I know an addendum for the datasheet was in the work. Please contact Freescale Support or your Freescale Sales Representative for updated information about these devices.

0 Kudos