imx53qsb amd-gpu(amd z430) minimum memory requirement.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53qsb amd-gpu(amd z430) minimum memory requirement.

1,111 Views
rayssadet
Contributor I

Hi:

Does anyone know the minimum memory requirement
for the amd-gpu in imx53qsb. ???
sure the board has enough memory but i am try to use
a scaled down version but so far up to 512MB i am getting
error from heavy graphics application.

Is there some documents stating this ??

thanks

:RAYS

Labels (2)
0 Kudos
2 Replies

836 Views
maxmustermann
Contributor I

BIG FAT WARNING:

Do NOT use the proprietary kernel / kgsl stuff. It's full of horrible security bugs and broken by design.

It gives the userland *FULL PHYSICAL* bus access - there's *NO SECURITY* anymore !

[imx53] WARNING! Do NOT use the proprietary GPU drivers / KGSL stuff - MAJOR RISK!

0 Kudos

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rays

as states i.MX53_START_Linux_BSP_Release_Note.pdf

gpu_memory =128M - memory reserved for the GPU.

IMX53_1109_LINUXDOCS_BUNDLE

also check attached document with memory usage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------