Dear community,
I have a question about L2.6.35_10.12_SSP_CLK_PATCH_UP patch modification.
[Background]
For TKT131240 errata ( SSP_SCK polarity setup issue in ROM ) ,
I have to use a L2.6.35_10.12_SSP_CLK_PATCH_UP patch.
And I would like to use VDD5V Source Only (AN4199 section 4.1.2.1) implementation .
[Question]
In order to work correctly with VDD5V Source Only,
how should I modify the patch file ?
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
It is need to use the patch for VDD5V configuration too.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It is need to use the patch for VDD5V configuration too.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------