Installing software encounter the following error. "No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534"
How to fix it?
Thank You.
Solved! Go to Solution.
This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community
This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community
Thank you. This solve the problems.
hi Lee,
what's your system platform? version?
Hi ZhangJennie:
I am using 32bit xubuntu 14.04.
Thank you.
Hi Lee,
Sorry little late with my feedback.
See you've solved the problem.
On my side I'm able to create an build a project created with the project wizard for FRDM-K64F.
My configuration is:
- Win 7 32 OS,
- VirtualBox,
- Ubuntu 14.04.1 (ubuntu-14.04.1-desktop-i386.iso)
- KDS V1.1.0.
After to have installed the tool as root, the tool must be launch as root too:
sudo /opt/Freescale/KDS_1.1.0/eclipse/kinetis-design-studio
This is working fine on my side.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------