ov5642 on sabre-tablet in ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ov5642 on sabre-tablet in ubuntu

1,155 Views
ehsanrezaie
Contributor I

Hi.

i am trying to run ov5642 module on sabre-tablet in ubuntu os.

is there any body that did it???

i made patch on board_mx53_smd.c file and load ov5642_cam and mxc_v4l2_capture modules .

but when run Cheese for capture it doesn't work .

Labels (1)
0 Kudos
5 Replies

733 Views
ehsanrezaie
Contributor I

ok .but RFS that he used is ubuntu 12.04 . and i am seeking for procedure of run camera on imx53 in ubuntu.

for exp: which one of .ko files should be loaded for run ov5642????   which one of module should be built in on kernel??? and other questions .

0 Kudos

733 Views
igorpadykov
NXP Employee
NXP Employee

Check IMX53 smd camera.  ERROR:  v4l2 capture: slave not found!

it explains procedure.

Please read carefully Linux documentation IMX53_1105_LINUXDOCS_BUNDLE

before posting next questions. All drivers : ov5642_camera.ko,ov5640_camera.ko,

ov3640_camera.ko, mxc_v4l2_capture.ko are located in ltib/drivers/media/video/mxc/capture

folder, if you take labour to buld image L2.6.35_11.05_ER_SOURCE   - you will find them there.

You can also look at another Ubuntu 14.04 i.MX53 :

i.MX53 Quick Start - Linux on ARM - eewiki

0 Kudos

733 Views
igorpadykov
NXP Employee
NXP Employee

Hi ehsan

please look at p.45 i.MX53 QSB Board Video

you can try with demo images below

L2.6.35_MX53_ER_1105_IMAGE

UBUNTU_RFS_DEMOIMG :

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

733 Views
ehsanrezaie
Contributor I

did you try by this RFS UBUNTU_RFS_DEMOIMG    and this kernel source L2.6.35_MX53_ER_1105_IMAGE . because in this RFS there is no required .ko  files(for example OV5642_CAM.so) and without them it is impossible that camera work correctly .

0 Kudos

733 Views
igorpadykov
NXP Employee
NXP Employee

Other customer tried, link below and that works

IMX53 smd camera. ERROR: v4l2 capture: slave not found!

0 Kudos