AnsweredAssumed Answered

K65 Max UART Baud Rate

Question asked by michaelsteffenfae Employee on Aug 7, 2014
Latest reply on Aug 14, 2014 by Hui_Ma

Question regarding the max UART baud rate on the K65 is that the input clock needs to be divided by 16, hence the max should be 60MHz (bus clock) / 16 = 3.75MHz.  Can anyone confirm this?

 

The K65 LPUART seems to remove the required divide by 16, but I assume that is to allow for the over-sampling feature.  What is the max baud rate on the LPUART?

 

Mike

Outcomes