Qt on Wandboard-solo with Yocto -Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt on Wandboard-solo with Yocto -Problem

660 Views
nileshkokane
Contributor I

Hello,

If anyone can help me to sought out the this issue to built up Qt on wandboard-Solo with yocto.
 



Based on the url  http://wiki.wandboard.org/index.php/Building_Qt5_using_yocto_on_Wandboard I altered the local.conf and the bblayers.confand gave a bitbake core-image-minimal with DISTRO_FEATURE_remove
  
I got the errors as posted  http://pastebin.com/hsMhT9f8.


Then to circumvent the errors I removed the DISTRO_FEATURE_remove from the local.conf
  and gave a bitbake.with this i got the errors as posted http://pastebin.com/QFu2Rw6G.

for the thirld time I tried to change the following
  


1) In /meta-fsl-arm/qt5-layer/recipes-qt/qt5/qtbase_%.bbappend
  

QT_CONFIG_FLAGS_append_mx6 = "${@base_contains('DISTRO_FEATURES', 'x11','-xcb',  ' -eglfs', d)}"
  
  

I replaced -no-eglfs with  -xcb


2)In  /bin/fsl-community-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase.in
  QT_CONFIG_FLAGS += " \
     -reduce-relocations \
    -shared \
    -silent \
    -no-pch \
    -no-rpath \
    -pkg-config \
    ${EXTRA_OECONF} \
"

-silent was deleted.
  

With this setup and without DISTRO_FEATURE_remove I gave i bitbake and was encountered with the errors as posted http://pastebin.com/V2fMF785
  


Please suggest to resolve this issue.

Thanks

Nilesh Prakash Kokane

Tags (5)
0 Kudos
0 Replies