AnsweredAssumed Answered

Maximum size of ldb in i.MX6DQ.

Question asked by Keita Nagashima on Aug 4, 2014
Latest reply on Aug 5, 2014 by igorpadykov

Dear Sir or Madam,

 

Hello.

Could you tell me the maximum output size of ldb with single channel mode in i.MX6DQ ?

 

Refer to MCIMX6DQRM(Rev.2).

Is this right? I consider that dual input data interface case is higher performance than single input data interface case.

=======

Overall: LDB supports rates needed by WUXGA 16:10 aspect ratio (1920 x 1200 @60 frames per second, data rate supported up to 170 MHz)

• For single input data interface case: Up to 170 MHz pixel clock (WUXGA1920x1200)

• For dual input data interface case: Up to 85 MHz per interface. (WXGA 1366x768 @60 frames per second, 35% blanking).

=======

 

Best Regards,

Keita

Outcomes