Does i.mx6DualLite's MIPI DSI interface support 1024X768 or 1280X800 LCD resolution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.mx6DualLite's MIPI DSI interface support 1024X768 or 1280X800 LCD resolution?

866 Views
dennishuang
Contributor I

Hi Sir,

    We plan to kick off a new project and use i.mx6's MIPI interface to drive 1024X768 or 1280X800 LCD panel.

Could it support those modes? We find the information of reference manual. It supports 160x120(QQVGA) to

1280X720(XVGA). Does the hardware limitation is 720 vertical lines? We are confused about it?


Thanks and Best Regards,



Dennis Huang

Labels (2)
0 Kudos
1 Reply

384 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dennis

yes hardware supports bigger resolutions (as 1280X800),

however fps may be less due to performance limitations.

1280X720 is given at 60fps.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos