iMX6 Clock Root Generator figures wrong or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Clock Root Generator figures wrong or not?

Jump to solution
948 Views
MichaelV
Senior Contributor II

Hi,

iMX6SDL/DQ RM section 18.5.1.5.4 Clock Root Generator.

The figures in that chapter show the locations of the Clock Gates. The following signals show no gate (cg) in the figure, but they do have a gate according to the CCGRn registers:

  • PCIE
  • VDO_AXI
  • CAN_CLK
  • UART

Is this a documentation error, or does it mean these signals are really different than the others (maybe gated at a later stage)?

Labels (4)
0 Kudos
1 Solution
624 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michel

correct description is given in CCGRn registers.


Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
625 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michel

correct description is given in CCGRn registers.


Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
624 Views
MichaelV
Senior Contributor II

So, just to confirm; the figures under section 18.5.1.5.4 Clock Root Generator should show (cg) for the PCIE, VD_AXI, CAN_CLK and UART signals? There is nothing "different" with the clock gating than any of the other signals, correct?

0 Kudos
624 Views
igorpadykov
NXP Employee
NXP Employee

Yes, correct

Best regards

chip

0 Kudos