Will imx287 support the capactive touchscreen?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will imx287 support the capactive touchscreen?

Jump to solution
560 Views
ask
Contributor III

Will imx287 support the capactive touchscreen?

I read imx287 will not support the capactive touch screen. Is it right?

Labels (1)
0 Kudos
1 Solution
442 Views
VladanJovanovic
NXP Employee
NXP Employee

i.MX28 supports resistive touch screens natively through built-in ADC.

For capacitive touch support, external touch controller connected via I2C or SPI is required.

View solution in original post

0 Kudos
1 Reply
443 Views
VladanJovanovic
NXP Employee
NXP Employee

i.MX28 supports resistive touch screens natively through built-in ADC.

For capacitive touch support, external touch controller connected via I2C or SPI is required.

0 Kudos