Hi all,
I noticed a tearing effect when using the wayland version of the 3.10.17 GA BSP. This is what I did:
1. Build the 3.10.17 GA BSP with wayland for sabresd board.
2. Start the weston egl example in fullscreen mode (“weston-simple-egl -f”)
You will see a tearing effect at the triangle’s sides which looks to me if there is no vsync.
Does the Freescale weston gal2d backend support vsync?
Hi,
Do you use multi-buffer for render? Single buffer will cause tearing, please use following command
export FB_MULTI_BUFFER=2
jack