If you mean address of the slave i2c device, then you can set it following way:
1. Using just one slave device - Bean Inspector -> Properties -> Slave address init. The address will be used automatically with each call of SendBlock, RecvBlock, etc.
2. Using more than one i2c slave devices. Use "SelectSlave" method to change the address of the slave device in your application. Address passed to SelectSlave method will be again used automatically with each call of SendBlock, RecvBlock, ....
Address will always be sent first when calling SendBlock method. After that data passed as parameter of SendBlock method will be sent.
I hope this will help you.
Martin