iMX53 SPI salve mode and DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 SPI salve mode and DMA

570 Views
charleshuang
Senior Contributor II

Dear guys,

If I want to set iMX53 SPI to slave mode and to use DMA , how can I do ?

Is there any reference ?

Is there one imx53 platform sdk ? (just like there is one imx6 platform sdk)

Best regards

Labels (2)
0 Kudos
1 Reply

365 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

there is no imx53 platform sdk, but you can use attached example

and i.MX6 SDK eCSPI SDMA example for writing own code (i.MX6 and i.MX5x

SDMA and eCSPI modules are similar). Hope this helps.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------