Header file for KL16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Header file for KL16

668 Views
chuckh
Contributor III

Hello,

Is the peripheral memory map header file the same for the KL26 and the KL16?  I can't find one for the KL16, which is what we're using, but the FRDM board says it's for both processors. 


Thanks.

0 Kudos
1 Reply

365 Views
adriancano
NXP Employee
NXP Employee

Hi,

The difference between this two devices is that the KL26 has the support for the USB module and the KL16 has not. In the attachments you can find the header file for both processors.

If you have installed CW 10.x you can find the header files for each processor in this path: <install_folder>\Freescale\CW MCU v10.6\MCU\lib\wizard_data\ARM\DataBase\derivatives

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos