error installing ds5_update-site.zip into DS-5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error installing ds5_update-site.zip into DS-5

Jump to solution
906 Views
rocketdawg
Contributor II

First, it complained about an old org.eclipse.core.runtime dependency.

I installed org.eclipse.core.runtime, and fixed that issue, and it still fails to install the plugin.

Cannot complete the install because one or more required items could not be found.

Software currently installed: Freescale MQX support for ARM DS-5 1.0.2.201307020935 (com.freescale.mqx.ds5.feature.group 1.0.2.201307020935)

Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found

Cannot satisfy dependency:

From: Freescale MQX support for ARM DS-5 1.0.2.201307020935 (com.freescale.mqx.ds5.feature.group 1.0.2.201307020935)

To: com.freescale.mqx.configuration.editor [1.1.6.201307020935]

i cannot find any (com.freescale.mqx.configuration.editor) install site or download

using 4.1 w/ patch 4.1.0.1

DS-5 5.19.0

Vybrid tower.

0 Kudos
1 Solution
496 Views
rocketdawg
Contributor II

This line:

Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found

means that MQX Configuration Editor is dependent on Eclipse v3.7 to 3.8.

DS-5 v5.18 and v5.19 uses Eclipse v4.3, so you have two options:

- Use DS-5 v5.17, which had Eclipse v3.7. You can find it in the "Older Releases" tab here: http://ds.arm.com/downloads/

- Contact Freescale for information on whether they're planning to update MQX Configuration Editor to support Eclipse 4.3.

or use this

https://community.freescale.com/thread/323233

View solution in original post

0 Kudos
2 Replies
495 Views
soledad
NXP Employee
NXP Employee

Hi David,

Please check the attached document and let me know if this helps.

In addition, according with the release notes Freescale MQX RTOS was compiled and tested with

DS-5 Starter Kit for Vybrid Controllers version 5.16.0

DS-5 Vybrid Controller Edition 5.16.0


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
497 Views
rocketdawg
Contributor II

This line:

Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found

means that MQX Configuration Editor is dependent on Eclipse v3.7 to 3.8.

DS-5 v5.18 and v5.19 uses Eclipse v4.3, so you have two options:

- Use DS-5 v5.17, which had Eclipse v3.7. You can find it in the "Older Releases" tab here: http://ds.arm.com/downloads/

- Contact Freescale for information on whether they're planning to update MQX Configuration Editor to support Eclipse 4.3.

or use this

https://community.freescale.com/thread/323233

0 Kudos