U-Boot on I.Mx35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot on I.Mx35

653 Views
m_f_vankessel
Contributor I

I'm trying to port U-Boot for an custom I.Mx35 board with only NAND-Flash, the board comes with an RedBoot bootloader.

Is there someone who has any experience with booting from NAND flash?

I have read some I.Mx configurations and I could only find one device booting directly from NAND (Karo - tx25, I.Mx25).

But I'm not sure if this will also work for the I.Mx35?!?

Max

0 Kudos
1 Reply

414 Views
Yuri
NXP Employee
NXP Employee

Please refer to app note AN4172 (U-Boot® for i.MX35 Based Designs)

http://cache.freescale.com/files/dsp/doc/app_note/AN4172.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos