NVCC_MIPI on 3P3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVCC_MIPI on 3P3V

Jump to solution
741 Views
mosmos
Contributor I

On Wandboard and SabreLite NVCC_MIPI is connected to 3P3V.

The datasheet IMX6SDLIEC sets the operating ranges for NVCC_MIPI from 2.25 to 2.75V.

Why is there a difference?

Manuel.

Labels (2)
0 Kudos
1 Solution
533 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip
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
534 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos