gstreamer in directFB image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer in directFB image

1,096 Views
zhencongtee
Contributor III

Hi,

I intend to test the gstreamer video decoding and camera streaming capability using the directFB image (bitbake fsl-image-dfb). However, I notice that the gstreamer in the dfb image is very minimal and does not have the elements like mfw_v4lsrc (camera input), vpudec (hardware video decoder) etc.

Is there an image in the bsp that can do what i required, running camera streaming and video decoding using gstreamer to directFB? Or i need to custom-made my image?

Thank you.

Regards,

Zhen Cong Tee

1 Reply

430 Views
gusarambula
NXP TechSupport
NXP TechSupport

I would recommend downloading the Yocto BSP release as it contains more codecs than the Community BSP. Are you working on the BSP release or the community BSP?

You may find the steps to download the i.MX6 BSP Release on the L3.10.17 i.MX6 Documentation Bundle available on the documentation page. Please look for L3.10.17_1.0.0_LINUX_DOCS (Linux 3.10.17 BSP & MM Bundle)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Then look for Freescale Yocto Project User's Guide.

Just to ease things the key information would be the repo which is:

$ mkdir fsl-release-bsp

$ cd fsl-release-bsp

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.0_ga

$ repo sync

$ MACHINE=< machine name> source fsl-setup-release.sh -b <build directory> -e <backend fb,

dfb, wayland, x11>

0 Kudos