i.MX6q Android 4.3 Kernel crash / unstable at 1.2Ghz (and 996Mhz).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6q Android 4.3 Kernel crash / unstable at 1.2Ghz (and 996Mhz).

1,255 Views
anthonydefeo
Contributor I

I am running the android_jb4.3_1.1.0 image on a Freescale MCIMX6Q-SDB board.

The system is running at 1080p resolution.

I have upped the frequency to 1.2Ghz by blowing the SPEED_GRADING fuse:

"imxotp blow --force 4 0x2b0302"

and setting the cpu frequency to max from android console:

echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor; echo 1200000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed;

At this speed, the system is unstable and the kernel will randomly crash with various oops messages (undefined instruction, unable to handle kernel paging request, unable to handle kernel null pointer reference, etc).

I am also running a build of android from source on multiple wandboard/technexion imx6q boards, and they all fail in the same way (some of them even fail at 996Mhz).

The system will crash randomly, but It seems to happen more often from the android settings->Data Usage screen.

All of the boards appear to be stable at 792Mhz.

We are developing a commercial product based on the wandboard/technexion, and this is a show stopper for us.

Any help or ideas would be greatly appreciated!

Thanks,

Tony DeFeo

Incredible Technologies, Inc.

Labels (3)
0 Kudos
4 Replies

685 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anthony

this speed fuse is blown on Freescale factory

(but not customer), after passing 1.2 Ghz qualification tests

and have special marking, for example MCIMX6Q5EYM12AC.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

685 Views
anthonydefeo
Contributor I

Thanks for the info, I didn't realize that the part was only rated at 1Ghz!

However, I am still having similar issues at 996Mhz, and the failure mode appears to be the same as when I run the part at 1.2Ghz except that it happens much more frequently at 1.2Ghz.

When I run the part at 792Mhz, I don't see the failure.

Any other ideas or help would be appreciated!

Thanks,

Tony

0 Kudos

685 Views
jiujinhong
Contributor IV

Hi Anthony,

did you fix this issue?

0 Kudos

685 Views
igorpadykov
NXP Employee
NXP Employee

Could you try linux ?

0 Kudos