Dear all,
I have boug
ht a P1010-RDB-PA from Freescale,and follow the DEMO to finish our board, but when I use CW for Power Architecture v10.3.3 to connect our board,it init failed. When I compare the log from IDE, it fail at reading memory,here is the log :
ccs_read_register
coreh = [serverh:0:cc_index:0:chain_pos:0]
index = 2032
count = 1
size = 4
value: ( size = 4)
00000000
but I check the DEMO, the log is here:
ccs_read_register
coreh=[servrh:0:cc_index:0:chain_pos:0]
index = 2032
count = 1
size = 4
value:( size = 4)
FFFFFFFC
So is there any problem at our board?Thanks!
Hello,
Try to make a simple application using CodeWarrior's wizard. Make sure
you select your hardware and from the project settings provide the correct
initialization file (P1010RDB_init_core.tcl, you will find it in your install path)
regards,
Catalin
Hello,
Thanks for your answer, but now we come to a new error:
Error launching test3-core00_RAM_P1010_Download
CCSProtocolPlugin : Secure debug violation
Here is some log form IDE,
ccs_config_server
serverh = 0
cc = 0
server_config = 0
value = 10230
ccs_config_server; ccs_error = 0
ccs_get_config_chain
serverh = 0
device_list: (size = 0)
ccs_get_config_chain; ccs_error = 0
ccs_config_chain
serverh = 0
cc = 0
device_list: (size = 1)
device[0]:: core_type=p1010(219)
ccs_config_chain; ccs_error = 39
Error message: p1010: Secure debug violation
ccs_get_subcore_error
serverh = 0
cc = 0
error = 57
chain_pos = 0
ccs_get_subcore_error; ccs_error = 0; duration=2 ms
ccs_in
coreh = [serverh:0;cc_index:0;chain_pos:0]
ccs_io addr: (size = 4)
0x00000000 0x00035b61 0x00000000 0x00000000
value: (size = 8)
01880000 00000200
ccs_in; ccs_error = 0; duration=2 ms
ccs_kill_server
serverh = 0
ccs_kill_server; ccs_error = 0
Could you kindly help us to debug this error? Thanks!
It seems recently several users met similar things on P1010RDB, is your USBTAP relative old? Some has avoid this using newer one. Also there is new version CW10.4 for public download, you may have a try.