i.MX6DQ Android BSP VPN support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ Android BSP VPN support.

Jump to solution
1,350 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about VPN with i.MX6Q Android BSP.

Our partner checked the work of VPN, but it did not work well with a setting even though Android BSP supports VPN according to i.MX6 D/Q and i.MX6 DL/S Android JB4.2.2_1.0.0-GA release.

Please see the detail as below.

=====

[Board]

MCIMX6Q-SDP

[BSP]

android_jb4.2.2_1.1.0-ga or android_jb4.3_1.1.0

[Procedure]

1. Launch Settings and select "Security" on android BSP after boot.

2. Select "Screen lock", and set "PIN".

3. Select "More..." in "WIRELESS & NETWORKS".

4. Select "VPN".

5. Tap "+" on upper right of screen.

6. Select type as "L2TP/IPSec PSK".

7. Input Name, Server address, IPSec pre-shared key, and tap "Save".

8. Connect VPN set in process No.7.

[Result]

If select L2TP/IPSec PSK in process No.6, it did not work well.

But if select PPTP, it worked well.

=====

[Question]

Q1. Does i.MX6 Android BSP (jb4.x) support VPN with "L2TP/IPsec"?

Q2. If the answer to Q1 is YES, did Freescale confirm whether it works well?

Q3. If the answer to Q1 is NO, do you have a plan to support VPN with "L2TP/IPsec" in following revision (KitKat BSP)?

Q4. Does i.MX6 Android BSP (jb4.x) support VPN with "IPSec Xauth xxx" and "IPSec Hybrid RSA"?

Best Regards,

Satoshi Shimoda

Labels (5)
Tags (1)
0 Kudos
1 Solution
856 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

The VPN feature is not hardware platform related, so in Freescale Android BSP, it should be same as Google default Android release.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
7 Replies
856 Views
satoshishimoda
Senior Contributor I

Please anybody give me a advice?

0 Kudos
856 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

I’m downloading android_jb4.3_1.1.0 BSP for testing the mentioned behavior.

Could you please tell me how did you test if it was properly working or not? Any tool/network/server that could be used for test the L2TP/IPSec connection?

Best regards!

/Carlos

0 Kudos
856 Views
satoshishimoda
Senior Contributor I

Hi CarlosCasillas,

If it does NOT work, the connection status in "Settings -> WIRELESS & NETWORKS -> More... -> VPN" as following images.

IMG_0157.JPG.jpg

IMG_0158.JPG.jpg

If it works properly, the connection status is changed to "Connected" instead of "Disconnected" or "Connecting".

Best Regards,

Satoshi Shimoda

0 Kudos
856 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

I have asked if jb4.x BSP supported "IPSec Xauth xxx" and "IPSec Hybrid RSA", and if we have plans to support "L2TP/IPsec" in following Android releases.

I will let you know when receiving a response.

Best regards!

/Carlos.

0 Kudos
857 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

The VPN feature is not hardware platform related, so in Freescale Android BSP, it should be same as Google default Android release.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
856 Views
satoshishimoda
Senior Contributor I

Hi Carlos,

Thank you for your reply.

OK, I understood Freescale does not modify the VPN function.

According to your reply, it is depends on Google Android release also whether KitKat BSP support VPN, right?

Best Regards,

Satoshi Shimoda

0 Kudos
856 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

Yes, it depends from Google; VPN functionality is the same than Google default Android release.

Best regards!

/Carlos.