Porting MQX to i.MX6 - Cortex A9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting MQX to i.MX6 - Cortex A9

915 Views
Rob_iMX6
Contributor II

Did anybody try it?

We intend to do it, using just one core of the i.MX6 and supporting SPI, I2C, USB (Device), Ethernet (100Mbit/RMII 50MHz) and EIM.

By using the Vybrid A5 as a starting point, this should be feasible.

Maybe someone has some comments on this? Any comments are more than welcome!

We are willing to share the ported code, if there is some interest.

Regards,

-Urs

Tags (1)
0 Kudos
2 Replies

284 Views
RadekS
NXP Employee
NXP Employee

We are currently working on MQX port for i.MX6SX. It will be released in near feature as standalone MQX release.


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

284 Views
RadekS
NXP Employee
NXP Employee

I would like to apologize. I forget mention that MQX port for i.MX6SX will be only for M4 core. A9 core will be not directly supported.

If you would like use MQX for A9 core, you can contact Freescale Professional Services:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

0 Kudos