Hello
I suspect you have an issue with paths settings.
The message "WARNING: The file c:\XXX\main.c is more recent than the corresponding absolute file" means that on your disk, the modification date for the file c:\XXX\main.c is more recent than the modification date of the .abs file.
Only reason I can see for that is:
1- You are building on a PC and debugging on another one and the two PC do not have the same
time/date settings.
2- You are not using the same paths when building and when debugging.
3- You are using recursive paths for building and there are several occurrence of the specified
source file in the tree
Can you check whether the paths specified in the debugger error window are the same as path specified in the IDE access Paths?
You can see the paths searched while debugging selecting File -> "Configuration" in the debugger.
Look at all the paths specified in the General Path environment setting.
I would try to remove all recursive path to remove any random behavior.
If this does not help, then I would recommend you to submit a service request for that.
Click
here to submit a service request.
Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.
Attach the generated .zip file to the SR.
CrasyCat