AnsweredAssumed Answered

issue with mux'd pins

Question asked by vinod Karuvat on Jul 2, 2014
Latest reply on Jul 3, 2014 by Dragos GALALAE

Hello,

 

I am using the KL04 chip (24 pins package).

I want to use the comparator module in this chip(pins 13,19,20 and 22).

Assuming I give the reference ('-') input to the pin 22 (so its a step down of a supply of 11V to a

KL04 compatible 3.3V.

 

But, this is muxed to SWD_CLK programming pin. This would mean that there might be an issue

with programming and/or debugging. How can this be solved. I am using the Multilink Universal from PE.

 

 

 

Vinod.

Outcomes