AnsweredAssumed Answered

Yocto media player using hardware decoder

Question asked by Zhen Cong Tee on Jul 2, 2014
Latest reply on Jul 8, 2014 by gusarambula

Hi,

I am trying to run some HD video on the i.mx6 SOLO in Yocto.

I tried the qt-media player and the "video" player that is build in in Yocto-x11, the CPU load runs up to around 30% when the video is playing.

However, when i use gst-launch command (gstreamer) through console, the CPU load is less than 10%.

 

From the above, i would think that the qt-media player and the "video" player in the Yocto is using software decoder, while gstreamer is using hardware decoder, and thus has the difference in CPU load.

 

Is there anyway we can get the qt-media player to use the hardware decoder? Or is there any player for Yocto that utilise the hardware decoder like gstreamer?

 

Thank you.

 

Regards,

Zhen Cong Tee

Outcomes