Dear Sir,
Our customer want to adjust Rset and Rload value to meet TV output level 1.6V.
Could you help check how adjust Rset and Rload value.
Thanks a lot,
We found Table 82 on i.MX6CEC.pdf Rev.6 10/2012
chapter 4.7.8.6.1 TV Encoder Performance Specification
Rset = 1.05 kΩ ±1%, resistor on VREFOUT pin to Ground
Rload = 37.5 Ω ±1%, output load to Ground
Full scale output voltage type=1.35V and MAX=1.45V
Solved! Go to Solution.
Hi Andy
this module is characterized only under conditions
given in Table 82 of Datasheet. So other output voltages are not guaranteed.
Sorry, seems one needs to add some external circuits for boosting output
voltage.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Andy
this module is characterized only under conditions
given in Table 82 of Datasheet. So other output voltages are not guaranteed.
Sorry, seems one needs to add some external circuits for boosting output
voltage.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------