AnsweredAssumed Answered

MKW01xx DIO0/DIO1 interrupt

Question asked by mircopizzichini on Jun 27, 2014
Latest reply on Aug 15, 2014 by Cesar Manzanarez Ayala

Hi

I'm using MKW01 with Radio Utility firmware. I've correctly routed DIO0/DIO1 to PTC3/PTC4, but when I want to send a packet, the only interrupt generated is the TxFifoLevel related to DIO1. My packet (10 byte length) is splitted in two blocks, but then I never received the PacketSent interrupt on DIO0.

1) Could it be a software problem? If there's a version for pre-production chip, I can test it on Reference Board

2) Does it still works without connections to PTC3 and 4?

Thank you

Outcomes