Hello,
I plan to build an appliance running Asterisk (pbx), based on P1020, as I'm very interested in the TDM support.
To start working on software with a P1020MBG-PC: it's FXS/FXO interfaces should be great to benchmark the TDM support on Asterisk (Dahdi). Next step would be to add ISDN support (PRI and BRI) on this TDM.
I can't find any support on how to port Asterisk to P1020, nor on a way to add P1020MBG SLIC/SLAC interfaces.
Has somebody already done something like this, and advises ?
Best regards,
Stephan
Hi Stephan,
Freescale SDK contains support for TDM and SLIC for P1020MBG-PC. You can visit Freescale Technical Information Center. Hope this helps.
Regards,
Sandeep
Hello Stephan,
If you are using Yocto SDK to build filesystem, you could download asterisk recipes from openembedded
recipes-isdn/asterisk in sysmocom-openembedded/meta-telephony (023ca5da04c53ef93ce7c933c2d362ad901ad..., download source tar ball into "sources" folder, then add package asterisk and build it into filesystem.
I am not sure whether this is what you want, if further assistance is needed, please feel free to let me know.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------