AnsweredAssumed Answered

Timer Unit; SetPeriodTicks, what is it based on?

Question asked by Mark Nordstrand on Jun 25, 2014
Latest reply on Jul 3, 2014 by Mark Nordstrand

The other day, I set up a TimerUnit with a period of 1ms.  In code I called SetPeriodTicks() with a value of 10000 and until recently it was responding in the OnCounteRestart event every 10 seconds.  Now it is responding every .2 ms.  It took a while, but I finally noticed that this is 10000 times the counter frequency.  Which of these should SetPeriodTicks() be using?  Rereading the description, I can see it being either way. 

Outcomes