Hi,
I'm trying to use the codesize tool available in the MQX 4.1 tools folder. However the html output gives me no information, as in the following image:
All itens are as above, with an '-' symbol. This is the command I'm using and the stdout output:
Do you have any idea on why this could be happening? I've tried searching another threads here without success.
Thank you!
Luiz Fernando
Solved! Go to Solution.
It should work.
However: Are you sure that you used CW compiler? GCC is currently not supported by this tool.
CW compiler/linker typically generate *.xMap file instead of *.map file.
Best Regards,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It should work.
However: Are you sure that you used CW compiler? GCC is currently not supported by this tool.
CW compiler/linker typically generate *.xMap file instead of *.map file.
Best Regards,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I can't test if it will work as a change of toolchain now will be hard, but you're right: I'm using GCC and haven't realized it is not supported!
Hope I can find something similar that works with gcc soon!
Thanks very much!
Luiz Fernando